Part Number: TUSB211RPTREVM
Other Parts Discussed in Thread: TUSB211, TUSB216I, TUSB216
Hello,
During the design with the TUSB211RPTREVM, our eye diagram doesn't seem to improve throughout the different EQ settings. We are currently only trying to improve the USB host's performance, without long cabling yet. Our goal is to use a 2 ft. cable when the design is complete, but we're not seeing improvement with a 6" cable.
Do you have any suggestions for us with what the issue could be? With and without the evaluation module, our eye diagram is very much the same. All indicators on the EVM suggest that the device is enabled and working properly. I've attached a sample of the eye diagram we are looking at without the EVM attached. Again, with it attached it is almost completely the same.

Thank You,
Zach Solheim