Part Number: DS110DF1610
Other Parts Discussed in Thread: USB2ANY, DS110DF410, DS125DF1610
HI,TI
1. How to generate the correct hex file?
When using retimer DS110DF1610, select EEPROM as the startup configuration mode, and have the target board (non DEMO board) and EEPROM chip Programming tools on hand. Now I want to generate a ". HEX" file in the "EEPROM page" of SigCon Architect, then burn it directly into the EEPROM chip, and configure the retimer to read the internal data of the EEPROM in the SMBUS master mode for itself work configuration. However, the data on the "EEPROM page" page of SigCon Architect cannot be updated. The EEPROM data generated by clicking the "Write to EEPROM Hex" button are all “00”, and the software is now in DEMO MODE . What is the problem? How to generate the correct hex file? Can you provide a generic hex file for reference?
The generated hex file data is 00: 
- Is the EEPROM size 64kbit (AT24C64) OK?
- Is there any rule or good method for debugging RX TX value? Can you share it?
thanks!
Best,
jack