Part Number: DS90UB929-Q1
Other Parts Discussed in Thread: TFP410, ALP, USB2ANY
Dear all,
I'm trying to configure a DS90UB929 device via I2C interface by using a microcontroller. The micrcocontroller is defined as the master device and when I'm sending the address word to the DS90UB929 device, I never received ACK signal from the 929.
ID voltage level is 0V (using 40 kOhm resistor pull down), so 929 adresse should be 0x18 for write operation.
Here is a screen copy of the I2C bus :

--> Normally, the SDA signal (yellow curve) should be pulled down to 0V during the nineth clock cycle.
On the picture, when SDA is configure as an input, the voltage level is 1.8V because of pull-up resistors (4.7 Kohm)
Could you, please help me to understand why it doesn't work ?
Per advance thank you
Best regards
Mickael C.