This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: Display configuration and screen flicker during test pattern

Part Number: SN65DSI84

Hello,

We are using the HDA1010WHPT-I-3GHI display along with SN65DSI84

Our DSI CLK is about 222.2MHz.

And using DSI Tuner we have configured following parameters. Are these configurations correct?

We use the test pattern config and see that the green and white lines are swapped compared to expected pattern as well as the flickers a bit.

Thanks in advance,

Sohil