This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711-SP: datasheet specifying characteristic impedance of each trace or differential impedance between the pair

Part Number: TLK2711-SP

Hello,

I have a question about signal routing on the TLK2711-SP.

 The datasheet specifies “Routing should be 50-Ω matched impedance and length for differential transmit and receive”

And Figures 8.4.2 and 8.4.3 show termination networks with two 50-Ω resistors between the differential signals.


Thus, I believe the datasheet is specifying the characteristic impedance of each trace, not the differential impedance between the pair. Is that correct?

THanks,

Adam