Part Number: P82B96
Other Parts Discussed in Thread: ISO1640, ISO1640-Q1, P82B715, ISO6742, ISO7742
Hi, I'm using the P82B96 for a simple I2C extender, but I am not reading anything on the TXRX or TYRY. I've tried increasing the 3.3V that pull up on TXRX and TYRY to 5V and reducing the resistor values without any luck. Is there a reference design for a simple application design reference that I could look at for a similar implementation? Pullups too strong or weak?
Thanks!