Part Number: DP83869HM
Hi,
Our board contains a FPGA and a DP83869HM PHY with SFP (RGMII to 1000Base-X).
On start-up, the PHY starts always OK. But after re-programming the FPGA, sometimes the PHY doesn't respond to the SMI bus.
On a MDIO read, I get always the same data (first data is random, all next data is the same as the first). It seems the PHY is frozen.
Only a power-cycle helps. The XI clock and Reset signal comes out the FPGA (hard-coded, not controllable) with a pull-down resistor.
Some timing measurements:
- The XI clock is started 17ms before rising edge of HW_RESET.
- The MDC clock is continuously, started 34us after HW_RESET. The frequency is 1 MHz. (The first MDIO action is a long time later).
Thanks in advance,
Jacob