Part Number: DS15BA101
Other Parts Discussed in Thread: DS15EA101
Hi,
I would like to connect two devices by SGMII, 1.25G with different voltage level as following:
TX side: device 1 transmit range is 225 - 525mvp-p to device 2 receive range 500 - 2400mvp-p
RX Side: device 2 transmit range 370 - 2200mv to device 1 receive range 100-600mvp-p
Please help me to choose the right part number.
If I need to calculate any resistor RVO, do you have a formula ? or maybe you can send me the Rvo I should use.
Since the values are typical, what is the +/- tolerance you can commit to ?
Thanks, Nir