This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS2200: clamping

Part Number: TVS2200


HI team,

1.can I see surge protection device as the ESD device but with very low dynamic resistance?

2.and why type-C power line recommended add a surge protection but data line normally don't?

  • Hi Fred,

    1. I'm not sure I understand your question. All our devices will provide some level of ESD and Surge protection. Most of our ESD/TVS devices have very low dynamic resistances. Are you looking for a device with lower dynamic resistance? 

    2. We also recommend data line protection. I'd suggest looking at our USB ESD & Surge Protection app note for device recommendations by USB type (2.0, 3.0, etc). 

    Regards,

    Sebastian 

  • Hi Muriel,

    if ESD also have surge protection like you said,

    then how to differentiate ESD and surge TVS?

  • Hi Fred,

    Some devices were designed with maximizing the surge current protection ratings while others will focus on a higher ESD rating. As I mentioned all ESD/Surge protection devices will provide some level of both ESD and Surge protection.

    If you're looking for devices with higher surge current ratings, the TVS family is a good option if you don't need 30kV ESD protection.

    We also have the TSM36A which will provide 30kV IEC ESD protection and 40 A of surge current protection (8/20us). 

    If you're asking when to use ESD protection vs. Surge protection this is application dependent. For USB, surge protection will mainly be a concern on the power line (Vbus).

    Regards,

    Sebastian