This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF230: question for DS250DF230

Part Number: DS250DF230

Hi Team,

The customer uses 3 pieces of DS250DF230 at the same time:

  • The first chip uses CPRI 9.8304Gbps or 24.33.24Gbps, and the CAL_CLK_IN of the chip is connected to the 30.72MHz clock
  • The second chip uses 25Gbps, and the CAL_CLK_IN of the chip is connected to the 25MHz clock
  • The third chip uses 10.3125Gbps, and the CAL_CLK_IN of the chip is connected to the 25MHz clock

Using SMBUS configuration, reading and writing registers is normal.

The customer wants to know how to quickly configure 3 chips and work at the corresponding speed? Could you share the corresponding register and the value that needs to be written to the register?

Thanks,

Annie