Part Number: DS250DF230
Hi Team,
The customer uses 3 pieces of DS250DF230 at the same time:
- The first chip uses CPRI 9.8304Gbps or 24.33.24Gbps, and the CAL_CLK_IN of the chip is connected to the 30.72MHz clock
- The second chip uses 25Gbps, and the CAL_CLK_IN of the chip is connected to the 25MHz clock
- The third chip uses 10.3125Gbps, and the CAL_CLK_IN of the chip is connected to the 25MHz clock
Using SMBUS configuration, reading and writing registers is normal.
The customer wants to know how to quickly configure 3 chips and work at the corresponding speed? Could you share the corresponding register and the value that needs to be written to the register?
Thanks,
Annie