Part Number: TUSB320
Hi,
Good morning!!
We are using TUSB320 device for the USB-C port configuration on one of our project, but we are facing issues to configure TUSB in host /device mode. Is there any changes need to do from software point of view for the device configuration. Our requirement with TUSB320 is to function as a host when connect to usb memory stick for the data extraction over USB2.0 and TUSB320 is to function as a device to interact with laptop for PC application.
Also we are using RT1062 microprocessor, please confirm the USB_ID or USB_Int pin can be connected to any GPIO pin or any dedicated pin for OTG USB controller is required.
Regards,
Sharon