Part Number: SN65DSI86
Hi
Would like to ask SN65DSI86 Dual-channel MIPI® DSI to embedded DisplayPort Can it work normally if only 1 channel is given?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It depends on the required resolution. If the DSI clk is less than 750MHz with the given resolution, then only channel A can be used.
Thanks
David