Part Number: TDP0604
Hi
Could you help check the below schematic and any need to adjust ,Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, Gareth,
I am working this now and will get back to you shortly.
Thanks,
Zach
Gareth,
The 1.8k pullups need to be on the HV_DDC_SCL/SDA, no need to have 1.8k pullups on LV_DDC_SCL/SDA.
For the DC-coupled output, AC_EN needs to be pulled low.
For pin-strap mode, HPDOUT_SEL needs to be pulled low to ground.
Is your source going to be DP++ AC coupled or DVI DC coupled?
Thanks,
Zach
Hi Zach
Is your source going to be DP++ AC coupled or DVI DC coupled?
>>> I have HDMI/DVI input, no DP input.
There is a pull-down resistor in the IC, if it is not used, can it be kept Floating or Pull-High externally instead of externally grounded?!

Gareth,
If the source output is DVI/HDMI, then you want to replace the TDP0604 input capacitors with 0-ohm resistor since DVI/HDMI is a DC-coupled interface.
To understand how to configure the pins that you referenced, please see: https://www.ti.com/lit/ml/slla589/slla589.pdf?ts=1680184377228&ref_url=https%253A%252F%252Fe2e.ti.com%252F
Thanks,
Zach