Other Parts Discussed in Thread: SN65HVD230
Please help!
I have a problem with rounded edges on the canH and canL coming from the sn65hvd230. I have attached screen shots. I have termination both on the node as well as the end of the cable each of 120 ohms. has anyone seen this or have any suggestions on how to change the edges and make them sharp? has anyone seen this problem before? I have a tight deadline on this, and this is the last piece to the puzzle so anyones input would be greatly appreciated.
Thanks in adavance,
Sean