Part Number: TRS3232E-Q1
Can the outputs be protected against short to battery in a 24V system? So the outputs should be protected up to 32V. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRS3232E-Q1
Can the outputs be protected against short to battery in a 24V system? So the outputs should be protected up to 32V. Thanks.
Hi Ovidiu,
Console side logic pins (ROUT and DIN) are not protected against a short to 24V or 32V.
The Bus side pins (DOUT and RIN) are protected to +/-13.2V (DOUT) and +/-25V (RIN)
So the bus side receiver pins can survive a short to 24V - the other pins cannot and none of the pins can handle a 32V short. There would need to be additional protection on the line to protect the IC pins in cases of shorts.
Abs max table from datasheet for reference:

Best,
Parker Dodson