Part Number: TRS3232E-Q1
So is the pin protected against 12V or not? If it is stated that the maximum allowable voltage is -6 +6, does that mean that the pin can withstand 12V if referenced to GND? And in an automotive design 12V is not enough because the range is wider. Actually the max voltage would be between 16V and 18V. So what about 18V?