Part Number: TCAN1463-Q1
Hello Eric,
the TCAN1463-Q1 datasheet mention on page 31 how to calculate the series resistor for the wake pin.
RSERIES is calculated using: RSERIES = VSUPMAX / IIO(WAKE)
IIO(WAKE) is not specified in the datasheet with max data only..
Using the 33k from the application circuit I calculate approx 1.36mA.
Will this drawn from the battery all the time?
Thanks
Martin