Part Number: MAX3221
Hi everyone
I tested according to the recommended circuit diagram in the specification, the chip 12 and 16 pins are connected to 3.3V, when the chip 8 and 13 pins are connected to the 232 serial port of the computer, the output voltage is normal and the output command is normal. When I disconnect the computer 232 serial port, the chip Dout output voltage is 0.
What is the problem?
Thanks!