Part Number: DS90UB638-Q1
Hi team,
(1) The DS90UB638 specification only mentions that 635 and 633 serializers are supported, assuming other serializers are used, such as 953, is it supported?
(2)
In addition, the customer has another requirement:
TI deserializer requirements:
1. Can be paired with DS90UB953
2. Support BT656/601/1120 output
3. Support 1920*1080@60P transmission
In 2 MP camera applications, it can be paired with DS90UB953 or MAX96717 and supports BT656/601/1120 output deserializers.
Which one does BU recommend?