Part Number: DS125BR800
Hello,
One customer need to confirm if DS125BR800 work with PRBS31 for ibert of xilinx?Is it suitable for Aurora 64/66 encoding? According to the datasheet it should only support 10G-KR is 64/66, which is the same as Aurora 64/66?
In addition, is there only one DS125BR800 in a high-speed data link?
His application is that: Two daughter boards A and C(both including DS125BR800) ,one backplane board B.
The signal flow direction: FPGA on daughter board A sends to board DS125BR800, 800 output signal goes through connector to backplane, signal leaves backplane.The DS125BR800, 800 output signal goes through the connector into Daughter Board B to the FPGA on Daughter Board B; the high speed data signal flow from Daughter Board B to Daughter Board A is reversed as described above.
The phenomenon:
1) In both PRBS31 and Aurora 64/66 test modes of ibert at 5Gbps, Daughter Board B is free of error but Daughter Board A has error code.
2) At 3.125Gbps, ibert's PRBS31 test mode, Daughter Board A and Daughter Board B receive no error code;
3) At 6.25Gbps, ibert's PRBS7 test mode, Daughter Board A and Daughter Board B receive no error code;
4) Remove the DS125BR800 from one of the daughter boards, keep only the DS125BR800 at the receiving daughter board on the high speed link, 5 Gbps ibert under PRBS31 test, no error code on the daughter board A/B;
Best regards
kailyn