Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TIC12400
I use the TIC12400 for monitoring individual relays (no matrix arrangement!).

I have configured the TIC12400 pins IN0 as "Sink" and IN10 as "Source". I want to use the "IN_STAT_COMP" register to read out whether the relay is switched or not. Is this arrangement possible to monitor a single relay?
Or does monitoring a single relay only work if
- the TIC pin IN10 configured as "Source" and the relay contact M1 connected to GND?

- Or the TIC pin IN0 configured as "Sink" and the relay contact M2 connected to Vs or Vbat?

Thank you in advance!