This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: Interfacing Two Switches for Single 4 Lane MIPI CSI,

Part Number: TS3DV642

Hello There,

We are currently designing a project that requires configuring different MIPI sources on a single 4-lane MIPI-compatible processor. Depending on the use case, we will switch to different ports. As shown in the image, Port B is selected in both switches (one switch port B is connected with 2 Lane MIPI + Clock, another switch port B is connected only with 2 Lane MIPI). Will splitting and connecting the MIPI through a switch cause any issues? like an imbalance of delay mismatches in between the traces? If so, how can we get past it?

Thanks,
Sakthivel