Part Number: ESD2CAN24-Q1
Hello Experts,
Can ESD2CAN24-Q1 to use for CAN FD(2MHz)? Or customer should consider ESD2CAN24FD-Q1?
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ESD2CAN24-Q1
Hello Experts,
Can ESD2CAN24-Q1 to use for CAN FD(2MHz)? Or customer should consider ESD2CAN24FD-Q1?
Best Regards,
Fujiwara
Hi Fujiwara,
Yes ESD2CAN24-Q1 has low enough capacitance to support CAN-FD. The FD version just has slightly lower capacitance, IEC ESD ratings and IEC surge ratings. I would choose the device with higher ESD/Surge ratings if the application requires that level of protection.
Regards,
Sebastian