Part Number: TUSB3410
Hi Expert,
UCstomer woudl to use TUSB3410 for design, but have some question as below:
if pull down VREGEN to GND, pull high RESET, and let SUSPEND floating, do you have any concern on that?
Regards,
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB3410
Hi Expert,
UCstomer woudl to use TUSB3410 for design, but have some question as below:
if pull down VREGEN to GND, pull high RESET, and let SUSPEND floating, do you have any concern on that?
Regards,
Mark
Hi Mark,
Below are the pin descriptions in the datasheet.

VREGEN pulled to GND will enable the 1.8V regulator.
RESET high will prevent the TUSB3410 from resetting
SUSPEND is an output, so floating will disable that output
Section 6.6 implies that VREGEN input tied low is no problem. I don't see any issues with not using the SUSPEND output and leaving it floating.

Regards,
Nicholaus