Hi team,
Could you please confirm such questions:
1. What are the input formats supported by the device? Currently, RGB666 and RGB888 are seen in the manual. Are there other formats? Can you help me to list all supported formats?
2. The datasheet shows the maximum condition and typical condition about the power consumption. I feel confused about what Icca and Icc stand for. If i want to calculate the power consumption, can i calculate consumption like that P=1.2V * 126mA? or P=1.2V*(126mA+52mA)?
Maximum condition: WQXGA 60 fps Dual-Link 2xDP at HBR2, PLL enabled; typical condition: WUXGA 60 fps 1xDP at HBR2, PLL enabled
3. Can the device support 4K? Because I saw that "4K equivalent to 120fps" is written in the feature description, and the 4K mode is not written in Table 13
YOURS
NAN