1. Does TI have single-channel DSI interface Serdes?
2. Does the DSI support virtual channels? Can achieve a single DSI interface output dual PFD-link function?
3.Does TI have an interface chip with USB DP port to FPD-LINK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Does TI have single-channel DSI interface Serdes?
2. Does the DSI support virtual channels? Can achieve a single DSI interface output dual PFD-link function?
3.Does TI have an interface chip with USB DP port to FPD-LINK?
Hi Xiaofu,
1. Does TI have single-channel DSI interface Serdes?
For 941AS, you can select the number of DSI lanes you need to use for your interface through Mode_Sel straps.
2. Does the DSI support virtual channels?
The 941 supports 4 virtual channels on the DSI. Please refer to section "8.4.6.4.2.2 Asymmetric Splitting With DSI VC-IDs" in the datasheet.
Can achieve a single DSI interface output dual PFD-link function?
Yes, it's possible to use single if lower BW or dual FPD-Link for higher BW to send the video through the FPD lanes.
3.Does TI have an interface chip with USB DP port to FPD-LINK?
We do have DP yes and we also have a newer DSI interface Ser.
For more information about newer generation FPD-Link devices here is the marketing contact you can reach out to:
TRANG NGUYEN (t-nguyen5@ti.com).
Regards,
Fadi A.