Part Number: LMH0303
Other Parts Discussed in Thread: LMH1219
Hi team,
Our customer use the FPGA to pull up or down the ENABLE pin. When the FPGA start to power up ,I/O will output some levels uncontrollably. They test the wave shown below:
In there test, the wave in yellow is the LHM0303_VCC and the wave in green is LHM0303_ENABLE. We can see that the ENABLE in green is pulled up at 1.45V for several seconds and last 380ms. And then the ENABLE is pulled up to 3.3V.
Would there be any potential risk for the device in such power on sequence?
YOURS
NAN