Part Number: TCAN4550
What kind of ripple is expected to be present on VCCOUT while CAN bus is running? We noticed some curving of the CANH signal and traced it to VCCOUT doing same.
Everything still works, so not sure if this is just the expected behavior.
If bus is off, VCCOUT is happy/steady.
The overall bounce is maybe 50mv in each direction
VSUP is at 12V and has 22uF and 0.1uF ceramics
FLTR has 1uF 10V ceramic
VIO is 3.3V has 1uF 0402 ceramic
VCCOUT has a 10uF 10V 0805 cap and no other load

Tried adding a second 10 uF cap to VCCOUT and it cleared things a little bit

Schematic: