This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I: Min value of MDC clock frequency

Genius 17995 points

Part Number: DP83848I

Hello,

I have a question for MDC frequency of DP83848;
The datasheet specifies it as 2.5MHz (TYP) and 25MHz (MAX). It doesn't specify the min value.
Isn't there no limitation for the min frequency? Is 1MHz supported?

Regards,
Oba