Part Number: TUSB4020BI
Other Parts Discussed in Thread: TUSB4041I
Hi Team,
Could you please comment on how to configure PIN35 and PIN36 of TUSB4020BI? The customer's requirements are as follow.
1. The system provides 3.3V and 1.1V to this device;
2. The upstream of the device is connected to the USB2.0 port, one of the downstream ports is connected to eUSB (similar to SSD), and the other is connected to a USB2.0 Type A.
3. Host can access TUSB4020BI through I2C, and the device is configured as SMBbus mode (1000 101);
4. The USB2.0 Type A interface has an eFUSE
Regards,
Hailiang