Part Number: TUSB4020BI
Hi team,
Support need
The scenario used by the customer has two levels of hub cascade connection, as shown in the figure below. The power-on time of Hub 2 would be earlier about ten seconds than Hub 1.
①.For the cascade connection of Hubs as shown in the figure below, do Hub1 and Hub2 have power-on sequence requirements? If Hub2 is powered on before Hub1, will the two devices(设备已) connected to Hub2 be fail to be recognized?
② If the Hub2 device cannot be recognized due to the power-on sequence problem, is there any way to avoid it in the software?

yours
nan