Part Number: TCAN1145-Q1
Hello team,
I ask some questions about the CAN_DR and FD_DR settings in the SW_CONFIG_1 register of TCAN1145-Q1. Would you please answer the following?
-. If the configured CAN DR is different from the data rate of the received WUF, is it recognized as a normal WUF or an error?
-. If the network is used as CAN FD 1Mbps (and arbitration is same as 1Mbps), how should CAN_DR and FD_DR be set to? CAN_DR=? FD_DR=?
Thanks,
Sam Lee