Part Number: TCAN1145-Q1
Hello,
What is POR? I guess it stands for Power On Reset and sometimes it is a voltage level also called as “POR level”, which is probably the same as VSUP(PU)R/VSUP(PU)F. However, I cannot find any meaningful difference from “Power Up” and UVSUP. I think all those 3 are effectively the same. Why do you treat them as different events? What difference should be kept in mind when the device is used?
In the figures 10-8 through 10, the device goes into standby mode anyway. No effective difference.

In “10.4.7.6.1 UVSUP, UVCC” the explanation is “If VSUP decreases more, the TCAN114x-Q1 shuts everything down as the POR level has been reach and when VSUP returns, the device comes up as if it is the initial power on.”. But the device is power off under UVSUP anyway.
In “11.2.2.1 Brownout”, Brownout is defined as “when VSUP is ≤ UVSUP but > POR state”. But what is meaningful in the figure is just ≤ UVSUP. POR state is not necessary here and effectively the same as UVSUP.
I tried hard to figure out what the difference is to find everything suggests they are effectively the same.
Thank you.
Regards,
Oguri (TIJ automotive FAE)