Part Number: DS250DF230
Hi,
I have a question about the DS250DF230ZLSR.
1. Do you have a graph or table showing the frequency characteristics of CTLE, VGA and DFE?
If you have one, please provide it.
2. If there is no table or graph for No. 1, could you tell me the range of effective CTLE Boost at Data Rate = 9.8304, 4.9, 2.4 and 1.2 bps?
For example, ”at 9.8304 bps, CTLE Boost can be set from how many dB to how many dB”.
Here's some background on asking the above question.
We are communicating at Data Rate = 9.8304 bps, and we have changed the setting of the EQ TABLE INDEX in the CTLE Boost Table from the default 0 (0.6 dB) to 18 (25.8 dB).
However, there was no change in the operation of the device, so we asked a question.
In addition, the other setting conditions are as follows:
・ADAPT MODE(REG_0x31[6:5])=0
Manual CTLE
・EQ TABLE INDEX:0~3
1) Channel-REG_0x2D <- 0x3C
2) Channel-REG_0x03 <- 0x00 EQ TABLE INDEX:0
OR Channel-REG_0x03 <- 0x01 EQ TABLE INDEX:1
OR Channel-REG_0x03 <- 0x02 EQ TABLE INDEX:2
OR Channel-REG_0x03 <- 0x03 EQ TABLE INDEX:3
・EQ TABLE INDEX:4~
1) Channel-REG_0x2D <- 0x38
2) Channel-REG_0x03 <- 0x00 EQ TABLE INDEX:4
OR Channel-REG_0x03 <- 0x40 EQ TABLE INDEX:5
OR Channel-REG_0x03 <- 0x50 EQ TABLE INDEX:6
・・・
OR Channel-REG_0x03 <- 0xEF EQ TABLE INDEX:18
Best Regards,
Nishie