Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: DS90UB953-Q1
Now we are tuning a video transfer solution which used DS90UB960-Q1 (deserializer) and DS90UB953-Q1(serializer).
So far, we can not get the video data in the main board, which is connected to DS90UB960-Q1 board.
Then we performed BIST test to confirm status of the hardware link.
We wrote the kernel code referring to P960_953_BIST_AllPorts.py in Analog LaunchPAD. The BIST test seemed to be running well, as there is no obvious error in the log.
But the main board still cant receive any data.
We have some quesions about the chip.
1. Register RX_PORT_STS1 (0x4D) in DS90UB960-Q1,
[1] PORT_PASS 1: Receive input has met PASS criteria.
We can read 1 in this bit, does it mean DS90UB960 can receive valid video data?
It not, how can we make sure DS90UB960 could get the video data well in BIST test?
2. Can we know if there is video data in coaxial cable by oscilloscope?
If there is video data in coaxial cable, we can see the waveshape of about hundreds mV?