This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044A-Q1: Total lead package inductance for input pin (VCC) of TCAN1044ADRBRQ1

Part Number: TCAN1044A-Q1
Other Parts Discussed in Thread: TCAN1167-Q1

We need Total lead package inductance for input pin (VCC) of TCAN1044ADRBRQ1 to set high frequency limit for Decoupling analysis to ensure power integrity. The package of TCAN1044ADRBRQ1 is VSON (DRB). Please provide details as soon as possible

  • Shanjai,

    We'll have to contact our design and packaging teams for this information as it is not readily available to us. We will respond back when we get information, which should be as soon as Tuesday next week. But, do you need this for the TCAN1044A-Q1 or the TCAN1167-Q1? I see in the thread you referenced that you're going to use the TCAN1167-Q1 in your design, but using the TCAN1044A-Q1 IBIS model for simulation. While the CAN bus simulation will be the same for both, the package inductance is likely to be different.

    Regards,

    Eric Hackett