Part Number: MAX3221E
Hi.
Please, could I receive a help regarding the RS232 transceiver MAX3221EIPWR?
The schematic is here. I have tried to explain everything I could directly in the PDF, its a single page.
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3221E
Hi.
Please, could I receive a help regarding the RS232 transceiver MAX3221EIPWR?
The schematic is here. I have tried to explain everything I could directly in the PDF, its a single page.
Regards.
Hi Jeferson,
So the RIN pin will be protected with the current scheme that you have - the DOUT pin will not be.
If the fault is sustained while the driver is in high impedance mode no practical value of RT will truly protect the device - as the driver will be high impedance - and under normal operation its sending data to a ~5k load - so any series resistance is going to create a voltage divider.
Ultimately the diode on the DOUT pin needs to be kept under there absolute maximum always - for short faults - pulse proof resistors at ~10 to 100 ohms should be used -but for sustained as you describe you need a lower clamping voltage.
Please let me know if you have any other questions and I will see what I can do.
Best,
Parker Dodson