Part Number: DS125DF111
Hi,
We are experincing various BER issue were we are using the re-timer for an SFP link. The SFP module is connected to a re-timer and from the re-timer is connected to an FPGA.
Since the features of the re-timer like CDR locking and jittering, CTLE and DFE adaptation is also done on the FPGA, we are exploring the option to simply bypass the re-timer so that the data from the SFPs will reach the FPGA intact.
To apply a bypass config to the re-timer, it seems that some of the DFE weights and gains for the CTLE has to be set Manually. Hence we need support to figure out the bypass config.
Best,
Mohammadreza Nakhkash