This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: Interface Communication

Part Number: SN65DSI86

Hi, 

I have one question about SN65DSI86 implementation.

With this convertor IC, I'd to access driver IC of eDP panel. How could I achieve it ? In the datasheet of SN65DSI86 (https://www.ti.com/lit/pdf/sllseh2), it described as follows:

"The SN65DSI86 also supports DSI generic read and write operation. Using DSI generic reads and writes, the external GPU can configure the SN65DSI86 internal registers and communicate with eDP panels. The DSI generic read and writes is also used for panel self refresh (PSR). In order to use the PSR feature, the eDP panel must support PSR and the GPU must support generating generic reads and writes without stopping the video stream. Generic reads and writes must be performed during video blanking time in order for PSR to work properly."

From above description, I think GPU can access eDP panels via MIPI I/F. But I can't find any information about it. How could I get the operation guide about it? Thnaks.

Chilun