This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84-Q1: sn65dis84 test pattern

Part Number: SN65DSI84-Q1

Hi ,

Could you help generate a dsi84 test pattern register setting?

LVDS:

1920 x 1080

dual lvds

24bpp

dsi blank:

hfp  64      vfp  70

hbp 32      vbp 8

hpw 32      vpw 8

Single lvds clk 71.6M

de polarity: positive,hs vs polarity: negative  

lvds channel : Format2

clock reference: csi

best regards,

jeff wang

  • Jeff

    You can use the attached DSI Tuner to generate the DSI84 register programming value.

    0647.DSI Tuner 2.1.zip

    Thanks

    David

  • my computer no allow install Java environment, so cannot install dsi tuner 2.1

  • Hi, 

    You can download the Java environment from this link, http://javadl.oracle.com/webapps/download/AutoDL?BundleId=44457

    I generated the DSI84 programming value assume RGB888 and DSI CLK frequency of 429.6MHz with divider of 6. I would recommend using the reference clock instead the DSI clock since the reference clock tends to have cleaner jitter than the DSI clock. 

    //=====================================================================
    // Filename   : DSI84_Programming_Value.txt
    //
    //   (C) Copyright 2013 by Texas Instruments Incorporated.
    //   All rights reserved.
    //
    //=====================================================================
    0x09              0x00
    0x0A              0x05
    0x0B              0x28
    0x0D              0x00
    0x10              0x26
    0x11              0x00
    0x12              0x55
    0x13              0x00
    0x18              0x6c
    0x19              0x00
    0x1A              0x03
    0x1B              0x00
    0x20              0x80
    0x21              0x07
    0x22              0x00
    0x23              0x00
    0x24              0x00
    0x25              0x00
    0x26              0x00
    0x27              0x00
    0x28              0x21
    0x29              0x00
    0x2A              0x00
    0x2B              0x00
    0x2C              0x20
    0x2D              0x00
    0x2E              0x00
    0x2F              0x00
    0x30              0x08
    0x31              0x00
    0x32              0x00
    0x33              0x00
    0x34              0x20
    0x35              0x00
    0x36              0x00
    0x37              0x00
    0x38              0x00
    0x39              0x00
    0x3A              0x00
    0x3B              0x00
    0x3C              0x00
    0x3D              0x00
    0x3E              0x00
    
    
    The PLL_EN bit and SOFT_RESET bit are not set as they need to be set per the recommended sequence defined in the datasheet

    Thanks

    David