Part Number: TCAN1145-Q1
Hi~ Team.
TCAN1145-Q1 is SPI interface and does it support both parallel and daisy chain connection when use multiple devices?
Just example, when use two TCAN1145-Q1,
Parallel connection : need two SS(chip enable) for each device enable and share SCK, MOSI, MISO lines.
Daisy chain : MISO->next TCAN MISO connnection.
If can't use daisy chain, is there any reason?
Thanks.