Part Number: SN65DSI86
Hi,
I have a question about SN65DSI86 application.
In 8.3.1 of the datasheet from this link https://www.ti.com/lit/gpn/sn65dsi86/ , the partial text is abstracted as following list.
The SN65DSI86 also supports DSI generic read and write operation. Using DSI generic reads and writes, the
external GPU can configure the SN65DSI86 internal registers and communicate with eDP panels. The DSI
generic read and writes is also used for panel self refresh (PSR). In order to use the PSR feature, the eDP panel
must support PSR and the GPU must support generating generic reads and writes without stopping the video
stream. Generic reads and writes must be performed during video blanking time in order for PSR to work
properly.
As the words above with colors, it describes SN65DSI86 can support DSI generic read and write to communicate with eDP panel.
But I can't find the information to access the back-end D-IC via DSI generic read and write. Can any one help to provide the control information or flow?
Thanks a lot.