Part Number: TMUXHS4212
Hello,
I have some application questions regarding the TMUXHS4212IRKST part.
- The proper connection for the RESVD1 and RESVD1 pins (reserved pins)
- SLLA552 checklist advises NC
- SLASEP7A datasheet says tie to Vcc
- The high-speed differential data connections to the MUX are AC coupled on all ports (we don’t have control of this)
- Datasheet advises a 10k bias connection to 0 to 1.8V
- Is any voltage in that range OK, or should it be biased at the center of range (0.9V)?
- Are special HF resistors needed for the 10K terminations for use at 10Gbps (most resistors show substantial impedance reduction at 5GHz)?
Thanks,
Adam