Part Number: TIOL1115EVM
Hello all,
I am working on developing an IO-Link device with the TIOL1115EVM.
With the evaluation board, i am not using the VCC out of this.
Is it necessary for me to connect the Enable via pull down resistors, wake via pull up resistor and TX also via pull up resistor ? or can i simply connect the TX to TX on MCU pin, RX on RX pin and Enable and wake as GPIO outputs from microcontroller pins. without any resistor in between ?