Part Number: TUSB1002A
Hi Brian,
is this an error that device RX is not connect to corresponding RX of the port?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1002A
Hi Brian,
is this an error that device RX is not connect to corresponding RX of the port?

Hi,
Polarity swapping is supported by the USB3 spec as a way to ease the board layout. The SSTX and SSRX pairs can be swapped and during SuperSpeed handshake, training sequences TSEQ are sent and the D10.2 symbol is used to detect if lane polarity inversion is done (refer to section 6.4.2 of the USB 3.0 spec).
Thanks
David
Hi David,
just for self-learning, is there other protocol that support polarity swapping like HDMI or DP?
there is no polarity swappng for DP and HDMI, maybe PCIe, but need to confirm.
Regards
Brain