We have connected the MIPI Re-timer between the camera and the Processor. Randomly the power supply to the MIPI re-timer is experiencing a dip in the voltage which is supplied by the module itself. Because of this we are experiencing problems in streaming the camera. The current rating of the Switcher used to power the MIPI re-timer is around 300mA . kindly provide a solution to this issue as soon as possible.