Part Number: TSC2017
Vdd=0Vのとき、C1(SDA)端子とD1(SCL)端子に入力できる電圧範囲は-0.3V~Vdd+0.3V、つまり±0.3Vですが、これは正しいですか?
外部3.3Vでプルアップすると半導体が壊れますか?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.