Part Number: DP83TC814R-Q1
Hello Expert,
I have questions of Datasheet's Table 8-15. Recommended 3-Level Strap Resistor Ratios for PHY address.
At first, I supposed that this table show pull-up resistor value's recommendation based on as ratio of internal-pull down resistor as like as 5.8k * 13, 5.8k * 4.
This is because, Table 8-16's name is Recommended 2-Level Strap "" Resistor.
However, if I followed above understanding pin voltage will exceed datasheet's voltage requirement for each mode.(e.g. mode2@3.3V=0.726~1.386V but internal pull-down * 13 and internal pull-down / 13 will exceed the requirement.)
So I calculate pin voltage as Table 8-15 as recommendation of resistor "value" but it seem that don't have enough margin against datasheet's voltage requirement for each mode.(e.g. mode3@3.3V=1.518~3.3V but it will be 1.86V(3.3V * 5.8 / (4.5 + 5.8)))
Therefore, would you tell me your recommendation for pull-up resistor for 3-Level Strap pin as "actual number"?
Thank you and best regards,
Kazuki Kuramochi