Part Number: AM26LV32E
Other Parts Discussed in Thread: AM26LV32, THVD1450
Dear Experts
While checking the operation of a circuit using AM26LV32EIPW and AM26LV31EIPW, the following events occurred.
I would like to ask the following regarding the fail-safe function.
[circuit]
・Master and Slave are 1:1 RS485 half-duplex communication (communication speed: 20MHz)
・Both Master and Slave use AM26LV32EIPW and AM26LV31EIPW, and they are all connected to the same bus.
・Each differential line is equipped with a 100Ω terminating resistor (there is no external pull resistor for each differential line. expecting internal fail-safe behavior)
[phenomenon]
・During the period from when the Master completes sending the frame to when the Slave sends the frame (*1), the differential input of the receiver is around 0V, and during this time the output of the line receiver momentarily changes from High to Low. Sometimes. The slave will mistakenly detect that it is a frame from the master. Occurs when the cable length is long.
*1: At this time, both Master and Slave negate "G" of the line driver, resulting in Hi-Z.
[What you would like to ask]
According to P7 of your document "TIA/EIA-485 (RS-485) Interface Circuit" (JAJA179), if you use a transmission termination resistor (about 100Ω), the differential voltage will be around 0V and the receiver state will be no longer switch
My understanding is that the internal fail-safe does not work well, but does the description in the above document apply to the AM26LV32E as well?
Best Regards,
Miyamatsu